AXIS#.MOTOR.TEMPSOURCE

Description

This parameter selects the connector used for the motor temperature measurement when the axis motor control algorithm does not use a position feedback (when AXIS#.MOTOR.TYPE = 2 or 10). The temperature sensor is a thermal resistor connected to the drive through a 2-wire input. The type of thermal resistor is set with AXIS#.MOTOR.RTYPE.

The range of available AXIS#.MOTOR.TEMPSOURCE values are determined by the set of drive connectors. The connectors that support temperature measurements are full 15-wire connectors (X23) and Smart Feedback Adapter (SFA) devices (X1 and X2 with SFA).

When AXIS#.MOTOR.TYPE is not 2 or 10, AXIS#.MOTOR.TEMPSOURCE is not used.

Versions

Action Version Notes
Implemented 02-06-01-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on drive model

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.TEMPSOURCE

500bh

23h

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.TEMPSOURCE

510bh

23h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6244

1

6244 (0x1864)

AXIS1.MOTOR.TEMPSOURCE

Unsigned8

Read/Write

Yes

71780

2

6244 (0x1864)

AXIS2.MOTOR.TEMPSOURCE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TEMPSOURCE

6244

Unsigned8

Read/Write

-